Other Parts Discussed in Thread: TMS320F28379D,
Tool/software: WEBENCH® Design Tools
Hi,
1. I was suggested that a buffer like SN74LVC541APWR is better to use between DSP (TMS320F28379D) and UCC21750 to protect DSP.
UCC21750 datasheet P30: A fault will be reported to the input side to DSP/MCU, which means the signals can be directly go to DSP?
2. Also a buffer like SN74LVC541APWR was suggested to better use between ADC signals and ADC pins of TMS320F28379D. I've never used before.
Does these MCUs like TMS320F28379D need a buffer for it? When do I need to consider this to protect the MCUs?
Thanks,
Hongmei