Part Number: TIDA-00620
Other Parts Discussed in Thread: DRV8701, , DRV8702D-Q1, DRV8320
I am interested in using an architecture similar to the TIDA-00620 to drive a 12VDC brush motor at 100A in a unidirectional application. I am concerned that the DRV8701 does not have enough output current to drive several high current mosfets in parallel. My application is not 4 quadrant, we only need to drive the motor in one direction. Braking would be nice but it is not necessary. Can you recommend the changes required to make the TIDA-00620 design operate up to 100A? Thank you.