This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00355: Specifications of Transformer and inductor

Part Number: TIDA-00355

Hello,

It is observed that 2 transformers: (part num: 750342670, 750342671) and one Inductor(part num: 750342669) are not available in the market.
So can you let me know the detailed specifications of 1)750342670 2) 750342671 3) 750342669

I couldn't find them in internet and if I get them from Wurth electronics it will cost me and takes time. 

So let me know the specifications of the 3 part numbers provided

Hope you do so.

Thanks.

Sandeep