Hello,
We developed a PCB based on latest gerber files of TIDA-01505. In the PCB there is a 3 pin header J14 in which it is mentioned to input Level Shifter Power Supplies +20V & -5V. Please confirm whether the we need to provide these power supplies externally. The design uses WA8759-AL transformer which is specified to provide +20V & -5V on its Auxiliary windings. Whether J14 has any significance if the transformer provides these supplies?