This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010000: UCC28740 Transformer Design

Part Number: TIDA-010000
Other Parts Discussed in Thread: UCC28600

Hi,

I am trying to redesign the reference design for a Motor Drive application with the following requirements: -

Input voltage 290–1000 VDC  
Output voltage 24 V (3 A), Iso. 5 V (2 A)  
Vop1 24V 24 V 3 A
Vop2 5V iso 5 V 2 A
Vaux aux 12 V 0.1 A
Output power 82 W Inclusive of all output rails

I got the following calculations for the Transformer design with Rcs = 0.38 ohm, Ipp_nom = 2A, Iocc_actual = 4A, Lp = 1290uH :-

Transformer Design Requirement Summary
PARAMETER VALUE UNIT COMMENTS
Nps 9.00   Turns ratio for primary to 24-V secondary
Nps_iso 39.00   Turns ratio for primary to 5-V isolated secondary
Nas 16.71   Integer turns reduced Nas from 17.93 to 16.71
Lp 1600.00 µH Operating frequency at full-load = 32 kHz

Could you help with the Transformer design?
I tried the same with 24V, 4A output in WEBENCH designer (doesn't support multiple output) and got the Core type - E32/16/9.

I am guessing the VS feedback and Line Sense current compensation and Output voltage feedback circuits will remain the same (from the calculations). Would cross regulation be a serious issue in this ?

Could you help to verify the same and also how to proceed ahead ?

Regards,
Rohit.