Part Number: TIDA-00449
Hello,
This is regarding TIDA-00449 BMS.
While charging the Li ion battery pack(10s4p) through BMS(ie. through Pack- terminal), what is the minimum and maximum current allowed through BMS(TIDA-00449)?
For example, is it OK to use 42V charger with 9A current or 3A current?
Will the BMS allow any current for charging the battery pack or is there any way to program the IC to make it possible for the need of our application(fast charging 9A or normal charging 4A).
Thanks