Hi,
i use Windows10 with .Net Framework (Vers. 4.7.2) and i have troubles to go in connection with the hardware.
First i installed DELTASIGMAEVAL-GUI-installer.exe and after that, i installed ADS131A04-dvcpkg.exe. All seems fine and also Generic Bulk Device Driver was installed sucessful.
When i open first Delta-Sigma ADC EVAL Tool it open, but if i connect the hardware -> no connection was found (Image 1)
When i open Delta-Sigma ADC EVAL Tool after i connect the hardware -> hardware connect, but no Addresses or Registernames are shown on screen (Image 2, 3)