Other Parts Discussed in Thread: TPS23753A
Hello,
The reference design PMP11107 is presented as a PoE class 3 application and for an input voltage range from 36V to 57V.
I would like to know if it is possible to supply the circuit with 12V and if this design can be used in class 0 as the TPS23753A is able to do.
Thanks, regards
Sébastien