This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01624: Options of selecting flexible substrate and ink

Part Number: TIDA-01624
Other Parts Discussed in Thread: CC2640, CC2541

Hello!

I am planning on implementing the reference design on a flexible substrate using silver ink. I have 125 um Kapton Polyimide as the substrate in mind. And I am going to use Ag-based ink with greater than 65% Ag weight concentration. Does anyone have any experience with implementing the design on Kapton? Or is there any recommended substrate suggested by the designers?

  • Hi Muhtady,

    Thanks for your question. 

    My understanding is that the effect of the substrate and using silver ink should only be on the impedance of the RF traces and the overall flexibility of the board. If you believe that 125um Kapton will be structurally sound enough and flexible enough for your intended design purposes then it shouldn't be an issue. Your PCB manufacturer should be able to provide some guidance in this area, or perhaps even a sample of the substrate material. 

    Also, you will want to calculate the proper thickness for the signal traces in the RF path for silver ink, the dielectric constant of your material, and the substrate thickness. There are RF impedance calculation tools online that should be able to help with this. Alternatively, most PCB manufacturers offer the option to control the impedance of certain traces, this is the best option. 

    Best Regards,
    Brandon Fisher

  • Hi, Brandon! 

    Thank you for the feedback. May I know in your reference design, which substrate and ink type were considered? And also what was the trace thickness, substrate's dielectric constant and thickness? It would be really helpful if you could provide this information, if possible.

    Best,

    Muhtady

  • Hi Muhtady,

    The total board thickness is 6.4mils. We used a polymide substrate which was 3.0 mils thick, with a dielectric constant of 3.3. The trace thickness for the RF portion was 6 mils, with all of the traces being copper. 

    Best Regards,
    Brandon Fisher

  • Hello, Brandon!

    Thanks again. I am a bit concerned with the printed antenna performance. Do you have any separate document stating the dimension and test results for the antenna? How should I approach the antenna issues? 

    Also, in the BOM file, C12 and C14 are zero in quantity. Is that alright? Because the footprints for the C12 and C14 are there in the layout. 

    Best,

    Muhtady

  • Hi Muhtady,

    Muhtady Muhaisin said:
    I am a bit concerned with the printed antenna performance. Do you have any separate document stating the dimension and test results for the antenna? How should I approach the antenna issues? 

    We do not have an additional document discussing the RF performance of the antenna, but in practice we found it to be around 40ft without doing any additional matching on the board.

    Its true that covering or folding the antenna can also affect the range, but this shouldn't occur in normal use as at least one side of the antenna should be left exposed when worn. If you want to minimize the possibility of folding, you could always add a stiffener behind the ground plane of the device. That would add some rigidity to the design, but should still be small enough that its not too uncomfortable to wear. 

    Muhtady Muhaisin said:
    Also, in the BOM file, C12 and C14 are zero in quantity. Is that alright? Because the footprints for the C12 and C14 are there in the layout. 

    The BOM is correct, C12, C14, and R6 were included in the design for an optional Pi-matching network that was not necessary for our purposes, so the parallel portion went unpopulated. For optimum range, these footprints can be used to perform RF matching while the device is worn. That way you get the maximum possible range out of the antenna. 

    Best Regards,
    Brandon Fisher

  • Hi, Brandon! 

    To avoid the variation in antenna performance, do you recommend the use of chip antennas? Do you have the experience of using any particular chip antenna with this circuit designed?

    Best,

    Muhtady

  • HI Muhtady,

    We did not attempt to use a chip antenna for this design, as the intention was always to make it as flexible as possible. Also, since it was Bluetooth based design we were pretty satisfied with the range we were getting for this application.

    That said, a chip antenna is an entirely viable solution, but you will have to account for its size when considering how a patch would be worn. You will also want to adjust the ground plane and elements of the layout depending on the specific chip antenna. 

    Best Regards,
    Brandon Fisher

  • Awesome!

    Is there any compatible chip replacement for CC2640 which will provide me with on-chip RF antenna solution in the ISM band? I couldn't clearly find one but I remember coming across one design implementation using TI CC25XX SoC which provided on-chip antenna. Do you have any suggestions regarding that or do you recommend any compatible alternate for CC2640 with on-chip antenna feature?

    Best,

    Muhtady

  • Hi Muhtady,

    I apologize for the delay. You should be able to use any 2.4 GHz antenna you can find. This TI design for the CC2541 uses one from Johanson. It would work with the CC2640 as well. 

    Best Regards,
    Brandon Fisher