This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

100W(or 50W/200W) Bidirectional DC-DC converter with user specified control algorithms

Other Parts Discussed in Thread: LM5170, LM5170-Q1

Hi,

I am looking for low power bidirectional DC-DC converter designs along with a controller with MATLAB/Simulink coding interface and can handle optimal control or optimization or advanced control algorithms. Intended for multiple input energy source (batteries and supercapacitors) applications with 12V to 24V(DC link) conversion.

I have found a TI application report similar to my applications using C2000 (attached). Can I use C2000 for advanced optimization-based control algorithms?

Kindly suggest appropriate controller, DC-DC converter designs,.. etc if available. Any further suggestions are highly appreciated.

Thank you.bidirectiona C2000 TI.pdf