Hi
How to modify this design PMP21404 for DC 12V in to AC 12V out 1A ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi PYTsai,
I am not sure I 100% understand your question. PMP21404 is a boost converter that provides a fixed DC output voltage of 221V at up to 0.87A.
The input range is 120V - 350V.
You would like to change the input to 12V DC?
And have the output be 12V AC?
If that is the case, it is a completely new design.
Thanks,
Robert