Other Parts Discussed in Thread: BQ76940, BQ76930, BQ76930EVM
Dear All,
TIDA-01093 schematic, is having low drain current Mosfet & high Rdson, can i replace it with other mosfets, with high Drain current Mosfet & Low Rdson eaisly without modifying its driver circuit ?
Also, what if i, plan to mount 10 mosfets for charging path & 10 mosfets for discharging Path in current design, instead of 3 mosfets for each path ? Will i need to change driver circuitry ?
Also am thinking to mount Mosfet whose specs are as follows:-
1.) Drain current 100A.
2.) Rdson 3m ohm.
3.) Vgs th 4v min.
My continous current through mosfet discharge path will be 100A, as am using 10 mosfets in parallel ,will use just 10A from each mosfet , which will help regulate temperature of mosfets as well.
Rohit