This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01093: Q24 and Q25 are source follower or not.

Part Number: TIDA-01093

Hello,

In TIDA-01093, Q24 and Q25 are source follower or not.

If it is source follower then output of RXD is equal to VCC_B when Q24 is ON and RXD will be GND when Q25 is ON as per my understanding.

if it is correct then give voltage at RXD.

Waiting for earliest reply.

Thanks,

Best Regards,

 Prathamesh Patil