Hi,
We are using TIDA-00281 reference design to develop a two wheeler EV. We are trying to run a 300W BLDC motor with this design.
I want to confirm if this design is suitable for commercial applications like an e bike.
Thanks..!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are using TIDA-00281 reference design to develop a two wheeler EV. We are trying to run a 300W BLDC motor with this design.
I want to confirm if this design is suitable for commercial applications like an e bike.
Thanks..!!!
Hello,
Thank you for the interest in the TIDA-00281. This design is targeting a 48V BLDC application up to 1kW, so a 300W application will be within the capabilities of the design. The listed devices should be available in commercial and Q1 grade. For automotive applications the Q1 rated devices are specifically used.
Confirm if this addresses your questions, or you can post additional questions on this thread.
Regards,
Hi Richard,
Thanks for the answer..!!!
We will make sure we use Q1 grade components.
Thanks..!!!