Part Number: PMP9766
Other Parts Discussed in Thread: TPS63020
Hi,
I read the document of PMP9766.http://www.ti.com/lit/ug/slva726/slva726.pdf
It says that "The TPS63020 buck-boost converter operates bidirectionally and is able to transfer energy from its input
to its output as well as from its output to its input." But in the datasheet of TPS63020, it doesn't say anything about the bidirectional energy transfer function. Does all the buck-boost have this function?
In the document, it says"The charge current is defined by the negative current limit of the TPS63020 buck-boost converter. Depending on the converters operating mode, either in buck mode or in boost mode, the negative current limit is typically between 0.6 A and 0.8 A."My second question: Does the TPS63020 charge the cap with constant volatge? Is the current between 0.6 A and 0.8 A enough to charge the cap?
Best Regards,
Wenxiu