Part Number: PMP9766
Other Parts Discussed in Thread: TPS63020,
Dear All:
I read the
in the 3.2 Backup Capacitor Charging Operation the file describe“ First, the converter must be in forced PWM mode. The converter is able to operate in the reverse direction only in this mode. To enable the forced PWM mode, the PS/SYNC pin must be programmed to a logic high level. The TPS63020 data sheet (SLVS916C) shows a detailed description of this mode pin. Secondly, the output voltage of the TPS63020 must be programmed to a lower value than the system voltage” I want to know if the PS PS/SYNC pin must be programmed to a logic high level, if the super-capacitor reach the 1.8V level, the IC to boost function, that the system can't charge the super-capacitor. Can you tell me how to charging Operation?