Part Number: PMP5291
Hello,
(1) Are three batteries connected in parallel considered as a single cell? If that's the case, then PMP5291 can be used to charge the battery, right?
(2) The customer wants to charge the batteries at 5A. I believe 5A is too high and can cause damage to the battery. Can you please advise maximum safe charging current?
Thank you for your help.