Part Number: TIDA-00792
Other Parts Discussed in Thread: BQ76200, , BQ76940, BQ78350-R1
Hi,
I have designed a BMS using BQ78350-R1, BQ76940 AFE and Bq76200 Mosfet Driver and my BMS is nearly the same as TIDA-00792 Reference Design. The Li-Ion battery pack with this BMS is working properly, everything about the battery pack is well. However, I have designed this battery pack for AGV (Automated Guided Vehicle) device. The AGV is operated by Lead Acid Battery without any problem but it is not operated by our Li-Ion battery pack. When we monitors the motor drivers inside the AGV using motor driver interface, drivers cut off the output because of the Over Voltage Alert. However, output of the battery pack is never cut off.
I think, in this case It is necessary to explain, the AGV' s motor drivers generate electric energy and it wants to charge it back to battery pack. (regenerative system). I am concerning that the problem arises from here. Because when I read the datasheet of the motor drivers, it says that the electric energy generated by motor drivers must be charged to battery pack or consumed across a shunt resistor.
Do you have any suggestion to solve problem or experience about that?
Thanks in advance.