Other Parts Discussed in Thread: UCC28180, UC2854B
Hi E2E,
We want to find a solution, Did you have any suggestion?
PFC controller IC:
Vin:3-Phase 220 Vac or 3-Phase380 Vac
Vo:600 VDC
Po:5 KW
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Julian,
You can consider using the UCC28180 or the UC2854B.
The webpages for these parts are located here:
Regards
John