This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/BQ25895: BQ25895

Part Number: BQ25895

Tool/software: WEBENCH® Design Tools

Hi,

             Can you please share with me Cadence allegro schematic symbol and footprint file of ic BQ25895 for schematic and PCB Design.

Regards,

Jitendra

  • Hi Jitendra,

    Please download the BXL from the ti site available under Quality and packaging.

    You can extract the symbol and footprint in the desired version by using ultra librarian free reader.

    Please note you need to extract the footprint from the bat file.

    Thanks and Regards,

    Atul

  • Hi atul,

                     thanks for your former answer. tell me one thing more

    1. once we do the register setting in BQ25895 for battery charging voltage/current and others parameters through the I2C and USB. it will be same for always even if power on/off of chip. i know this this will happen but still  i want to conform by you.

    2. we want use it individual. it will not use with microcontroller or processor continue. it can be used individual after program by micro controller or microprocessor.

    3. According to the user manual of OF BQ25895 , A Device named EV2300 can be used for programming of BQ25895. is this application open source. could you send link for this.

    4. what about pin no.9 (CE) . this pin can be put high forever becouse we are not using micro controller with it to make it high or low repeatedly.

    5. PMID and System output can be used same time at their full load define. is system output  through battery whether  is VBUS or not and pmid output always through VBUS ?

    Regards,

    Jitendra

  • Hi Jitendra,

    Yes, the register setting will be present even after power off.

    Thanks and Regards,

    Atul