This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TMS320C6678: An edma example test failed

Part Number: TMS320C6678


Tool/software: WEBENCH® Design Tools

Hi everyone,

I need an edma example without os. I found one in mcsdk_02_01_02_06 \ pdk_C6678_1_1_2_6 \ packages \ ti \ csl \ example \ edma . But this example tests failed. The information shown in console is following:

[C66xx_0] **************************************************
******************* EDMA Testing *****************
**************************************************
Debug: Testing EDMA(0) Ping-Pong Test (Global) Region for Channel 0...
Error: Verification (Source1/Destination1) Failed
Error: Testing EDMA(0) Ping-Pong Test (Global) Region for Channel 0 FAILED

I have not modified the example, so where is the problem?

Many thanks in advance!

tf