Part Number: TIDA-00364
Other Parts Discussed in Thread: CSD19536KCS, CSD19535KCS,
Hi,
I am currently working on the 48V,5kW PMSM motor inverter drive.
I am trying to implement the same system with through hole mosfets. Now we are considering the CSD19535KCS,CSD19536KCS parts for hardware implementation.
if we consider CSD19535KCS part,it can carry a continuous current of (as per the datasheet) 133A. Our requirement is 133A continuous current and overloading current of 250A for 2min, switching frequency :20kHz.
For this we are planning to use 3 Mosfets in parallel.
In this configuration, we are getting 3.53W(Rds_on: 3.6m ohm) conduction loss and 10.64W (rise and fall time assumed as 100ns each)switching loss per FET. So the total inverter power loss is around 255W.
we are getting junction temperature of 76.34 deg cel for maintaining the inside air temperature of 65 deg cel.
But in the application note I can see 5 parallel mosfets (200A rated) are used for 5kW inverter system. May I know How you are choosing number of parallel mosfets for this application?
For our specifications, Is 3 parallel mosfets are sufficient for optimum operation?
Looking for reply at earliest.
Thanks & Regards,
Kalyanraj D