Part Number: TIDA-01471
Other Parts Discussed in Thread: ADS127L01, ADS1274, ADS1278
Hello,
we want to use more than one TIDA-01471 to read multiple IEPE sensors simultaneously. At the moment we have six boards connected to the Controller board and the DRDY line of one of the TIDA-01471 is used to start reading data from all ADCs via SPI. The data transmission works fine, but after a few seconds the DRDY signals are asynchronous and we need to resync the ADCs to prevent data loss.
We tried to send a stop command followed by a start command, but this causes a delay time of about 2.7 ms before the next DRDY signal (with 32kSPS). According to the ADS127L01 datasheet, this delay is caused by the wideband filter used by default in this design.
Is it possible to switch to the low latency filter instead of the wideband filter without modifying the layout? The delay should be around 20 us using the low latency filter, which seems acceptable.
Or is there another way to synchronize the ADCs?
Thanks a lot,
Kind regards
Patrick Oetken