Other Parts Discussed in Thread: UCC21540
I would like to simulate gate drivers switching two IGBTs with a variable dead time. Using TINA is there a way to add a dead time in between switching the top and bottom IGBT?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: UCC21540
I would like to simulate gate drivers switching two IGBTs with a variable dead time. Using TINA is there a way to add a dead time in between switching the top and bottom IGBT?
Hi, Frazer,
There are numerous ways to do this... Two that come to mind:
1. Put an RC in front of the logic input to the driver. This will effectively delay the signal coming in.
2. Put a gate resistor between the driver and the IGBT. This will delay the switching of the IGBT. You can put a diode in series to make the delay asymmetric.
Do you have a particular gate driver you're looking at? We have some with built-in dead-time generators (UCC21540 for example).