This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS563200: WEBENCH can't run simulation when Vin set to 5V and Vout set to 3.3V

Part Number: TPS563200

Tool/software: WEBENCH® Design Tools

Hi Team,

May I know why TPS563200 simulation doesn't work in Webench base on below input/output requirement:

1. Vin min: 4.75V

2. Vin max: 5.25V

3. Vout: 3.3V

4. Iout: 2A

BR.

Wiky