This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00961: TIDA-00961

Part Number: TIDA-00961

Hi,

I am giving 30V 50hz input,i am not switching any switches(MOSFET and GaN FET)and Control card also . The waveform after the diode D101 with respect to AGND should be half wave. But the waveform is comming wrong the screen shot of the same is attached below and average voltage should be Vm/pi but it is comming more than that. But if i isolate circuit after the thermistor(R101) by opening R101 the wave is comming correct. 

Thanks

yashwanth