This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS53647: Selectable number of phases

Genius 12865 points
Part Number: TPS53647

Tool/software: WEBENCH® Design Tools

Hello Team,

1) is it possible to adjust the number of phases for a TPS53647 design? Webench only allows 4 phases designs?

2) If I enter Vin=12V, Vout=1V, Iout=30A from the product page http://www.ti.com/product/TPS53647 I get a message that no valid operation point can be found.

Thanks and Best Regards,

Hans