Tool/software: Code Composer Studio
I am not able to run the example code. Specifically, SimpleBLEPeripheral_motorMonitorWakeup function in simple_peripheral.c is able to return when the system starts. But in the second time that it is triggered by a timer, this function does not return. Problem 2, the example code seems to not enable power saving, it is always working with a current around 65mA.