Tool/software: WEBENCH® Design Tools
I use a battery with a 18650 lithium battery and no temperature sensing pins.
Is it appropriate to use the BQ21040 as a charger?
The temperature sensor function of the BQ21040 is not used.
If this feature is not needed, a fixed 10kΩ can be placed between TS and VSS to allow normal operation.
IS there possible i placebetween TS and VSS to allow normal operation. then without 10kΩ thermistor?
http://www.ti.com/cn/lit/ds/symlink/bq21040.pdf P14