Part Number: PROCESSOR-SDK-OMAPL138
Other Parts Discussed in Thread: OMAPL138
Tool/software: WEBENCH® Design Tools
Hi
Steps
1.Install CCS9.1 (CCS9.1.0.00010_win64.zip) to C:TI.
2.Processor-SDK-ti-processor-sdk-rtos-omapl138-lcdk-06.00.00.07-Windows-x86-Install.exe) installed in the default folder
3.run setupenv.bat at c:tiprocessor_sdk_rtos_omapl138_6_00_00_07.
4.run benchmarkProjectCreate.bat at c:tiprocessor_sdk_rtos_omapl138_6_00_00_07demosaudio-benchmark-starterkit.
5.Check environment variables with the set command.
4. An error occurs in the item.
Detecting all projects in PDK and importing them in the workspace c:\ti\PROCES~1\demos\AUDIO-~1\\BenchmarkProjects
Detected Test Project: Benchmark_FFT_lcdkOMAPL138_c674ExampleProject
指定されたパスが見つかりません。
Copying macros.ini
指定されたファイルが見つかりません。
I don't know the cause.
Thank you for reading to the end.