This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/OMAP-L138: ROTS/OMAP-L138/lcdk-06.00.00.07-Windows-x86-Install:Arranging linker script.

Part Number: OMAP-L138

Tool/software: WEBENCH® Design Tools

Hi

I use a sample of bigtime introduced in bios_6_75_02_00 to make sure.

I'd like to rearrange the linker script to locate the program from DDR to the Shared RAM area.

But, It is recreated (overwritten) in the build process. Which underlying files should I fix?

I check the map file created by link.cmd at build time, the program remains located in the DDR.

Thanks for reading.