Part Number: TIDA-010024
Hello,
I am currently working with the 6lowpan_mesh_ti_15_4_cc1312_tirtos_ccs project file. Inside the app_task_node.c file, there is the following code:
I am currently trying to use the debug_push configuration and believe that this is controlling the timer which sends data every 10 seconds. I would like to change this so that the application sends data when an event occurs (i.e. a trigger from a microphone).
How can I change this code to instead send data when something like a trigger occurs instead of a timer?
Any help is greatly appreciated.
Thanks,
Grady