This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools: EM1402 Evaluation Module

Tool/software: WEBENCH® Design Tools

Our team bought two pieces of boards named TIDA-00817.But I have a question about the scenario how the circuit achieves the goal of charging or discharging the cell.

1、Is the 12V supply as the donator to charge one of 16 cells when the cell was charged?The module is 12V supply?

2、Is the 12V supply as the accepter to discharge one of 16 cells when the cell was discharged?The module is 12V supply?

3、Is the 12V supply is a switching power supply or a big cell?Whether the 12V supply is OK as a switching power supply?

Looking forward to your replies!