This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/UCC28070: Webench/UCC28070

Part Number: UCC28070

Tool/software: WEBENCH® Design Tools

Trying to design a PFC circuit by Webbench power designer. For both 400V 2A and 400V 8A the calculated default switching frequency ist 205.48kHz.

Switching to user preferred frequency at configuration options it is not allowed to have more than 30kHz. Why?