Part Number: TIDA-01501
Hello,
the Simulation results using the TINA model of UCC28180 provided with the Project, show that the Input current and also the Output voltage reach a very high value at the very beginning of the Simulation( the Input current, the curent flowing in the supply reaches about -900 A, and Vout reaches about 1500 Volt). I would like to ask you please if this performance is related to the design of the compensator? How can one solve this to avoid Problems with the Hardware when implemented?
Thank you very much.
Kind Regards,
Amr