This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP8896: High efficiency, isolated POE design with short (<13 mm) flyback transformer

Part Number: PMP8896

I want to implement the PMP8896 reference design: http://www.ti.com/tool/PMP8896, in my own design; however, I have strict constraints on my flyback transformer height, it must be < 13 mm. Can you recommend a replacement that is shorter than the transformer spec'd, pn: NA6223-AL, which is 13.7 mm?

The reason I like this design is b/c of high efficiency, i.e. ~90%, at my typical power consumption. I am OK with other recommended designs, and my power spec is only 7W. So, my requirements are: 7W max and efficiency optimized (+90% desired) at 4W as an isolated design.

Regards,
will