Part Number: TIDA-00643
Other Parts Discussed in Thread: TMS320F28027, DRV8305
Hello,
I am referring to the reference design TIDA-006643 which specifies a current limit of 15 amps. I am trying to design a version which can handle way more current. The MOSFETS in the design can handle more current. So I was wondering which components limit the current to 15 A. I have two assumptions. The first assumption would be the layout of the board itself or the rating on the current sensing resistors ?
I was wondering if there is anything else that will needs to be replaced.
Thanks