This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS53119: Iocp and Rtrip calculations

Part Number: TPS53119


Tool/software: WEBENCH® Design Tools

How does the Webench tool calculate the value for the Rtrip resistor and the resulting Iocp values?  Calculating the Iocp value with the Rtrip resistor value from Webench based on the datasheet calculations produces Iocp values which are much larger than necessary to the point of making the over current protection useless.

Is there anyway to see what the Iocp value Webench think it is using for the design?

  • Hi Robbie,

    here are the details for Rtrip calculation is done in the following way:

    Step 1: Itrip is calculated from the chart number four in data sheet page 7.:

    Step 2: Over current protection is set at minimum of 1A.

    Step 3: Vtrip is calculated from datasheet equation 7:

    Step 4: Rtrip = Vtrip/Itrip.

    Hope this helps you resolve your problem. I'll be closing this thread for now. Please post your calculations if you are still observing the mismatch. your new post will reopen this thread.

    Regards,

    Vishwanath

  • Hi Vishwanath,

    In step 1, you have found a datasheet error.  While the title says Figure 4 is the TRIP Pin Current vs. Temperature, this is incorrect and the chart is just a copy of Figure 3 with the Title changed.  In multiple place, including Electrical Characteristics on Page 6 and in the description of Overcurrent Protection on Page 15, the datasheet says there is slope versus temperature of 4700 ppm/C.  Also please note Figure 4 Y-axis is labeled as OVP/UVP Threshold.

    However, my question is actually a little different.  Webench calculates a value for Rtrip but does not offer any information on Iocp.  When I use the equation in Step 3 to calculate Iocp based on the value of Rtrip provided by Webench, Iocp is very large. 

    The first thing I did was check my calculations versus the Typical Application in section 8.2.2.  Using equation 7 with the values from 8.2.2 of Rtrip=20k, Itrip=10uA @ 25C, Rdson=1.1mOhm from CSD86350 datasheet,  Fsw=500kHz, L=0.44uH, Vin=12V, Vout=1.2V, and then calculating Iocp=25.18A.  The table in 8.2.2.1 shows that Iover=25A which matches the calculated value of Iocp=25.18A.  This confirmed that my calculations in a spreadsheet do in fact match the datasheet.  This also confirms that my selection of the Rdson value from the CSD86350 is matches the values used in the Typical Application.

    Next to find Iocp in my application because Webench does not output the overcurrent value.  Using equation 7 with the values from Webench of Rtrip=25.5K, Itrip=10uA, Rdson=0.7mOhm from CSD86360 datasheet, Fsw=650kHz, L=1.5uH, Vin=12V, Vout=5V and then calculating Iocp=47A.  Note, I selected the same Rdson value which the datasheet application note in 8.2.2 selected.  The problem is my application only has a maximum current of 15A DC and the simulations from Webench show the current waveforms of the inductor never get over 17A.  Calculated Iocp=47A versus typical application of 17A peak current means the overcurrent protection is basically useless.

    My questions are multiple,

    1.  Why does Webench set such a high value for Iocp? 

    2. What value for the Rdson of the CSD86360 does Webench use?

    3. Why does the datasheet set Iocp=25A for an 8A application?  

  • Hi Robbie,

    I've raised the request to modify the data sheet image. Thanks for noticing it.

    1. Wenech sets Iocp = 1.3*Iout. but limits it to minimum of 1A.

    2. Rds is a function of temperature and driver voltage. 0.7 mOhms is the typical ZDS value for the condition given in CSD86360 data sheet. We need M2 RDS for Rtrip calculation.

    3. We are consulting with the applications team for this device to find more information regarding Rtrip calculation and Iocp setting.

    Please let us know if you have any further queries.

    Regards,

    Vishwanath

  • Robbie,

    The TRIP voltage needs to be greater than 0.2V and less than 3V.

    Rtrip x Itrip   20kx10uA is 0.2V   With the low on resistance fets, current limit is higher. 

  • Hi David,

    Sounds like all my calculations are correct but this opens a different line of questions. 

    As Rdson of the Sync Fet has a direct and in this case negative impact on the actual current limit threshold if the Vocl=0.2V, are there any other methods to lower the actual current limit?

    Design is maximum 15A design but with the design from Webench the Iocp calculates to 37A.

    Thank you, Robbie

  • Hi Robbie,

        We will add the Iocp calculated value to be displayed in the opval section of the WEBENCH. At this point, I am not sure if there is a way to lower the current limit apart from increasing the Rdson of the LS FET. Anyway, will check and get back to you shortly.

    Regards,

    Gerold

  • Hi Robbie,

        At the moment, increasing Rdson of the LSFET is the known way to get the current limit lower.

    Even with Vtrip of 0.2V, the accuracy can have a +/-32% variation as per the datasheet.

    Do you want us to give you alternate part number recommendations?

    regards,

    Gerold

  • Hi Robbie,

         Just wanted to check if you need further assistance with this issue.

    regards,

    Gerold

  • Hi Gerold,

    No, at this time I do not require any further assistance.  This can be closed.

    Thank you, Robbie