This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM25118: The simulated output is not obtained in hardware setup

Part Number: LM25118

Tool/software: WEBENCH® Design Tools

Sir,

We tried implementing the circuit with LM25118 as obtained from WEBENCH. But we did not get the desired output 28 V. We are getting 50 V as output. Please suggest a solution for this issue. The circuit diagram is attached with this.

Regards,

Sithara

sithara.pendios@gmail.com