I'm trying to use a UCC21530 gate driver to simulate a buck converter.
The driver is taking in a square wave input of 5 volts and outputs a square wave of 20V which is used to switch a MOSFET.
The gate driver is operating properly.
The buck converter has a duty ratio of 0.4.
The buck converter works fine as long as the drain voltage of the MOSFET is lower than the gate voltage. If the drain voltage is higher than the gate voltage the output of the transistor is capped at 8 volts which is 40% of the gate voltage. I tried this with different MOSFETs from different companies and they all gave me the same result.
Here is the schematic:
VG1 and Vg2 are the input to the driver.
Vm1 and VM2 are the output from the driver.
VM3 is the output of the converter.
VM4 is the input of the converter