Part Number: TIDA-010042
Greetings,
I am working on design "www.ti.com/.../TIDA-010042" given by TI. In the schematic there are 2 sensors- TMP303CDRLR(for temperature sensing) and OPT3001DNPR(for sunlight intensity). At same link under software link I found the software for given design. In the code in main() Init_I2C(); function was commented and there is no use of I2C related variables in code.
My queries are:-
(1) Why exactly we want to calculate temperature and sunlight intensity using stated sensors? I am aware that these factors affect output power of solar panels but anyhow we are calculating MPPT then what is the need of monitoring temperature and sunlight intensity?
(2)If monitoring temperature and sunlight intensity is important then where to find the complete software related with this design ? If not important then can I remove 2 sensors from the design?
Thanks
Best Regards
Bhushan