This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010039: Request for the CPL file for assembly purposes

Part Number: TIDA-010039

Hi Team,

Our customer is requesting for the CPL file (Component Placement File for the pick and place machine) for TIDA-010039.
Please let us know if this file is available to share with the customer.

Thanks!

Jonathan

  • Pick Place for TIDA-01606E4_POWERCARD(001).txtHi Jonathan,

    Please share the attached file with the customer. Let me know if this is in the format needed by the customer. I can share the CPL file for the two daughter cards once you confirm this.

    Best Regards,

    Ram

  • Hi Ram,

    Thank you very much for this file.
    I will now share this with our customer and will get back to you once confirmed that this is the format the customer needed.

    Regards,

    Jonathan

  • Hi Ram,

    The customer confirms that the format you sent is what he is looking for.
    We are happy to share with him also the other files, so I will wait for it.

    Another question from the customer if available to answer:
    Are there specific requirements for the thickens of the copper layers on the PCB? Or does 18µm suffice for the the outer layers.

    Best Regards,

    Jonathan

  • TIDA-01606E4_Gate Driver_Pick.xlsx

    Altium Designer Pick and Place Locations
    C:\MyTI\TIDesigns\TIDA-01606\TIDA-01606\AltiumWorkspace - Release\TIDA-01606E4_ISOHVCARD\Project Outputs\BOM_TID\TIDA-01606_HV_CardE4(001)_TI-BOM.txt
    
    ========================================================================================================================
    File Design Information:
    
    Date:       29/11/19
    Time:       21:26
    Revision:   Not in VersionControl
    Variant:    001
    Units used: mil
    
    Designator Comment             Layer       Footprint         Center-X(mil) Center-Y(mil) Rotation Description                                                                                                                                         
    U1         TI-TPS22944DCK5     TopLayer    DCK0005A_N        200.000       560.000       90       "Low-Input Voltage 100 mA Current Limited Load Switch, 400 mOhms rDS(On), -40 to 85 degC, 5-pin SC70 (DCK), Green (RoHS & no Sb/Br)"                
    R6         CRCW04020000Z0ED    TopLayer    0402              250.000       670.000       360      "RES, 0, 5%, 0.063 W, AEC-Q200 Grade 0, 0402"                                                                                                       
    R5         Resistor            TopLayer    0603              210.000       317.707       180      "RES, 2.20 k, 1%, 0.1 W, 0603"                                                                                                                      
    R3         Resistor            TopLayer    0603              318.115       739.260       360      "RES, 47 k, 5%, 0.1 W, 0603"                                                                                                                        
    R2         ERJ-3GEY0R00V       TopLayer    0603              210.000       440.000       180      "RES, 0, 5%, 0.1 W, AEC-Q200 Grade 0, 0603"                                                                                                         
    C5         885012206095        TopLayer    0603              210.000       378.788       360      "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C2         885012206095        TopLayer    0603              290.000       560.000       90       "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C1         TAJA106M010RNJ      TopLayer    3216-18           380.000       540.000       270      "CAP, TA, 10 uF, 10 V, +/- 20%, 3 ohm, SMD"                                                                                                         
    DC-1       PBC02SGBN           TopLayer    Sullins_PxC02SGBN 1700.000      160.000       180      "Header, 2.54 mm, 2x1, Gold, R/A, TH"                                                                                                               
    DC+1       PBC02SGBN           TopLayer    Sullins_PxC02SGBN 2740.000      160.000       180      "Header, 2.54 mm, 2x1, Gold, R/A, TH"                                                                                                               
    U5         PTLV9061IDCKR       BottomLayer DCK0005A_N        300.000       790.000       180      "World's Smallest Amp 10MHz, RRIO, 1.8V-5.5V op-amp delivers high performance for challenging systems, DCK0005A (SOT-SC70-5)"                       
    U3         TLV70433DBVT        TopLayer    DBV0005A_N        2000.000      917.449       180      "Single Output LDO, 150 mA, Fixed 3.3 V Output, 2.5 to 24 V Input, with Ultra-Low IQ, 5-pin SOT-23 (DBV), -40 to 125 degC, Green (RoHS & no Sb/Br)" 
    R29        Resistor            BottomLayer 0603              398.701       845.551       270      "RES, 15.0 k, 1%, 0.1 W, 0603"                                                                                                                      
    R27        Resistor            BottomLayer 0603              1610.018      739.967       180      "RES, 39, 5%, 0.1 W, AEC-Q200 Grade 0, 0603"                                                                                                        
    R26        Resistor            BottomLayer 0603              1740.018      739.967       180      "RES, 3.16 k, 1%, 0.1 W, 0603"                                                                                                                      
    R25        Resistor            BottomLayer 0603              578.701       815.551       180      "RES, 4.70 k, 1%, 0.1 W, 0603"                                                                                                                      
    R24        Resistor            BottomLayer 0603              798.701       815.551       180      "RES, 4.70 k, 1%, 0.1 W, 0603"                                                                                                                      
    R23        ERJ-3EKF1000V       BottomLayer 0603              170.000       760.000       180      "RES, 100, 1%, 0.1 W, AEC-Q200 Grade 0, 0603"                                                                                                       
    R21        Resistor            BottomLayer 0603              578.701       735.551       180      "RES, 4.70 k, 1%, 0.1 W, 0603"                                                                                                                      
    R20        Resistor            BottomLayer 0603              798.701       735.551       180      "RES, 4.70 k, 1%, 0.1 W, 0603"                                                                                                                      
    R19        Resistor            BottomLayer 0603              1610.215      815.518       180      "RES, 39, 5%, 0.1 W, AEC-Q200 Grade 0, 0603"                                                                                                        
    R18        Resistor            BottomLayer 0603              290.197       615.551       180      "RES, 7.50 k, 1%, 0.1 W, 0603"                                                                                                                      
    R17        Resistor            BottomLayer 0603              420.197       615.551       180      "RES, 0, 5%, 0.1 W, AEC-Q200 Grade 0, 0603"                                                                                                         
    C22        Capacitor           BottomLayer 0603              468.701       845.551       90       "CAP, CERM, 0.01 uF, 16 V, +/- 10%, X7R, 0603"                                                                                                      
    C21        Capacitor           BottomLayer 0603              170.000       700.000       360      "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C20        Capacitor           BottomLayer 0603              688.701       775.551       90       "CAP, CERM, 0.01 uF, 16 V, +/- 10%, X7R, 0603"                                                                                                      
    C19        Capacitor           BottomLayer 0603              1430.000      780.000       270      "CAP, CERM, 0.01 uF, 16 V, +/- 10%, X7R, 0603"                                                                                                      
    C18        Capacitor           BottomLayer 0603              200.000       860.000       90       "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C17        Capacitor           BottomLayer 0603              878.701       1025.551      0        "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C16        GRM21BR61H475KE51L  BottomLayer 0805_HV           884.701       933.000       0        "CAP, CERM, 4.7 uF, 50 V, +/- 10%, X5R, 0805"                                                                                                       
    C15        Capacitor           BottomLayer 0603              1383.252      921.551       180      "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C14        Capacitor           BottomLayer 0603              350.000       550.000       180      "CAP, CERM, 0.01 uF, 16 V, +/- 10%, X7R, 0603"                                                                                                      
    U4         AMC1311DWVR         BottomLayer DWV0008A          1138.701      775.551       180      "Precision, 2-V Input, Reinforced Isolated Amplifier, DWV0008A (SOIC-8)"                                                                            
    U2         SN6505              TopLayer    DBV0006A_N        530.000       830.000       180      "Low-Noise 1 A, 420 kHz Transformer Driver, DBV0006A (SOT-23-6)"                                                                                    
    T1         750313638           TopLayer    Wurth_750313638   1140.000      817.449       360      "Transformer, 340 uH, SMT"                                                                                                                          
    R7         ERJ-3GEY0R00V       TopLayer    0603              500.000       720.000       180      "RES, 0, 5%, 0.1 W, AEC-Q200 Grade 0, 0603"                                                                                                         
    R10        RC0603JR-07330RL    TopLayer    0603              2458.504      1060.000      360      "RES, 330, 5%, 0.1 W, 0603"                                                                                                                         
    R9         ERJ-3GEY0R00V       TopLayer    0603              2318.504      1060.000      360      "RES, 0, 5%, 0.1 W, AEC-Q200 Grade 0, 0603"                                                                                                         
    R1         ERJ-3GEY0R00V       TopLayer    0603              500.000       600.000       180      "RES, 0, 5%, 0.1 W, AEC-Q200 Grade 0, 0603"                                                                                                         
    L2         74279228260         BottomLayer 0603              878.701       1095.551      180      "Ferrite Bead, 26 ohm @ 100 MHz, 6.5 A, 0603"                                                                                                       
    L1         742792662           TopLayer    0603              2188.504      1060.000      360      "Ferrite Bead, 1000 ohm @ 100 MHz, 0.6 A, 0603"                                                                                                     
    D2         B0520LW-7-F         TopLayer    SOD-123           1520.000      690.000       180      "Diode, Schottky, 20 V, 0.5 A, SOD-123"                                                                                                             
    D4         Zener               TopLayer    SOD-123           2424.504      910.145       270      "Diode, Zener, 5.6 V, 500 mW, SOD-123"                                                                                                              
    D3         150060VS55040       TopLayer    WL-SMCD-0603      2510.000      930.000       90       "LED, Green, SMD"                                                                                                                                   
    C8         885012206095        TopLayer    0603              1690.000      710.000       360      "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C7         C3225X7R1H106M250AC TopLayer    1210_280          1550.233      817.551       180      "CAP, CERM, 10 uF, 50 V, +/- 20%, X7R, 1210"                                                                                                        
    C13        C3225X7R1H106M250AC TopLayer    1210_280          2150.000      890.000       90       "CAP, CERM, 10 uF, 50 V, +/- 20%, X7R, 1210"                                                                                                        
    C12        GRM21BR61H475KE51L  TopLayer    0805_HV           2261.402      910.000       90       "CAP, CERM, 4.7 uF, 50 V, +/- 10%, X5R, 0805"                                                                                                       
    C11        885012206095        TopLayer    0603              2340.000      910.000       270      "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C10        C3225X7R1H106M250AC TopLayer    1210_280          1750.000      880.000       90       "CAP, CERM, 10 uF, 50 V, +/- 20%, X7R, 1210"                                                                                                        
    C9         885012206095        TopLayer    0603              1850.000      920.000       270      "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C6         885012206095        TopLayer    0603              840.000       830.000       270      "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C4         885012206095        TopLayer    0603              500.000       660.000       360      "CAP, CERM, 0.1 uF, 50 V, +/- 10%, X7R, 0603"                                                                                                       
    C3         C3225X7R1H106M250AC TopLayer    1210_280          730.000       697.370       90       "CAP, CERM, 10 uF, 50 V, +/- 20%, X7R, 1210"                                                                                                        
    D1         B0520LW-7-F         TopLayer    SOD-123           1520.000      940.000       180      "Diode, Schottky, 20 V, 0.5 A, SOD-123"                                                                                                             
    LBL1       THT-14-423-10       TopLayer    Label_650x200     2261.402      500.355       0        "Thermal Transfer Printable Labels, 0.650" W x 0.200" H - 10,000 per roll"                                                                          
    J1         61300411021         BottomLayer Wurth_61300411021 670.000       160.000       180      "Header, 2.54 mm, 4x1, Gold, R/A, TH"                                                                                                               
    R4         ERJ-3GEY0R00V       BottomLayer 0603              1750.000      510.000       90       "RES, 0, 5%, 0.1 W, AEC-Q200 Grade 0, 0603"                                                                                                         
    D5         CDSOD323-T03SC      BottomLayer SOD-323-Bi        1510.000      780.000       90       "Diode, TVS, Bi, 3.3 V, 10.9 Vc, SOD323, 2-Leads, Body 1.9x1.45mm, No Polarity Mark"                                                                
    R11        MMU01020C3323FB300  BottomLayer MMU_0102          2740.000      910.000       360      "RES, 332 k, 1%, 0.2 W, AEC-Q200 Grade 0, 2.2x1.1mm"                                                                                                
    R12        MMU01020C3323FB300  BottomLayer MMU_0102          2568.000      910.000       360      "RES, 332 k, 1%, 0.2 W, AEC-Q200 Grade 0, 2.2x1.1mm"                                                                                                
    R13        MMU01020C3323FB300  BottomLayer MMU_0102          2396.000      910.000       360      "RES, 332 k, 1%, 0.2 W, AEC-Q200 Grade 0, 2.2x1.1mm"                                                                                                
    R14        MMU01020C3323FB300  BottomLayer MMU_0102          2224.000      910.000       360      "RES, 332 k, 1%, 0.2 W, AEC-Q200 Grade 0, 2.2x1.1mm"                                                                                                
    R15        MMU01020C3323FB300  BottomLayer MMU_0102          2052.000      910.000       360      "RES, 332 k, 1%, 0.2 W, AEC-Q200 Grade 0, 2.2x1.1mm"                                                                                                
    R16        MMU01020C3323FB300  BottomLayer MMU_0102          1880.000      910.000       360      "RES, 332 k, 1%, 0.2 W, AEC-Q200 Grade 0, 2.2x1.1mm"                                                                                                
    R22        MMU01020C3601FB300  BottomLayer MMU_0102          1840.000      780.000       90       "RES, 3.60 k, 1%, 0.3 W, AEC-Q200 Grade 0, 2.2x1.1mm"                                                                                               
    
    Hi Jonathan,

    I am attaching the Pick and Place file for the 2 remaining cards.

    It is recommended to use 2Oz copper (70um thickness) for this design for all layers.

    Best Regards,

    Ram