Part Number: TIDA-01385
Hello
I have a questions regarding TIDA-01385 refference design for energy harvesting. I'm currently working on energy harvester project. The energy that will be harvested is magnetic field from power line, with the current flows is about 100 A to 400 A. I will use the CT as energy harvester, and TIDA-01385 as circuit to harvest the energy. Could it possible to recharge the battery of TIDA-01385 through the CT?
Can I have a contact to order TIDA-01385?
Thank you,
Sara