Tool/software: WEBENCH® Design Tools
Hi Team,
I am trying to simulated the LM61460-Q1 under the following conditions:
Vin: 9V - 19V
Vout: 5V
Iout: 4A
Ambient Temp: 30
When I switch to 2.1MHz switching frequency, the design will not update due to lack of phase margin. Can I know what the phase margin is under those conditions? I am surprised the phase margin is so low since those operation conditions seem fairly reasonable. Are there any conditions where 2.1MHz operation is acceptable?
Thank you,
Jared