Part Number: TIDA-01480
Other Parts Discussed in Thread: LM3881
Hello,
I'm posting on behalf of my customer.
We are analyzing the FPGA’s XCZU3CG, XCZU4CG and XCZU5CG for this project. I took the power sequence from the Xilinx DS 925 Zynq UltraScale+ MPSoC Data Sheet: DC and AC Switching Characteristics and currents from the XPE spreadsheet. Our Current values are higher than what is seen on TI's processor power webpage for the same model. Our project calculation is near 0.85V/10A and 1.8V / 1.5A.
My power system is based on the TIDA 01480. I have concerns regarding the necessary time between the power sources energizing/ramping up. I have the ramp of each power source, but not the information of any necessary wait time between the activation of each power source. Or if I can activate each power source after the subsequent power source, just respecting the ramp time.
Aside from the rail sequencing, can you let me know about the timing specifications for each supply in TIDA-01480? How are the individual ramp times factored in here?
Thanks,
Tom