Part Number: PMP21112
Other Parts Discussed in Thread: TAS3251, , PMP9774, PMP11769
Hello.
When i'm using the TAS3251 in combination with the PMP21112 Boost Converter, which Signal is connected to the PWM-tracking-Input of the PMP21112 Eval Board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Mr. Landgraf,
I can't see the TAS3251 directly generating the PWM signal to control the output voltage of the boost converter;
this will need some additional circuitry. A peak detection of the input AF envelope might be used here to modulate
the output - PMP9774 shows such an approach.
PMP11769 shows a solution w/ dual boost plus 2x TAS3251, but there is no AF envelope tracking implemented.
Best regards, Bernd Geck