This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/UCC28C43-EP: UCC28C43-EP

Part Number: UCC28C43-EP
Other Parts Discussed in Thread: TL431

Tool/software: WEBENCH® Design Tools

Flyback 33V 2.6A TI.TSCWBDesign 33V Flyback.pdfI have a web bench design for a 75V to 395V DC input and output of 33V@2.6A with opto feedback DCM

I have replicated the design in Tina TI (Free and Cloud)

1. The design does not startup with the opto configured as per web bench design. There could be an opto model issue which i am not sure off.

2. It does startup if the Vref on the opto is dropped as done by R8

3. The output is not regulated with opto feedback.

4. With various design constraints the opto proposed to be used is SFH-617A-2x009T

4. With a direct feed back from output 1 (R4 and R5 ) instead of opto output. The system has an output but not constant. This could be because of the compensation network values not being  matched to non isolated design.

The web bench design and TINA simulation attached.