Part Number: TIDA-01580
Other Parts Discussed in Thread: AFE4900
Tool/software: Code Composer Studio
I have made some demo boards TIDA-01580 and I got wave form from TIDA-01580 Application.exe. The ECG signals could be extracted although they are very weak signals,but the PPG (green ,red, IR)signals are just noises. The voltage drop is 1.8V 0.9V 0.6V for green diode red diode and IR diode.Thanks a lot, if anyone could give some advises .