Part Number: TIDA-010042
Hi,
The Design TIDA-010042 while testing,we have faced the following issue.
We are connected the Battery at a voltage of 12.1V and applying the Panel Voltage of 13V-14V, at this stage Battery is charging with a Current of 0.4A to 0.5A.
Later if we increase/decrease the Panel voltage(with a variation of 0.2V to 0.5V) then it exit from the charging mode and also increase the Panel voltage Linearly.
Thanks & Regards
Gangadhar P