Other Parts Discussed in Thread: CD74HC238, TPS65651
Hello,
I want ESD data i.e (HBM,MM,CDM) for the below 2 parts.
TPS65651RTER & CD74HC238PWR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Umesh,
I have the data below for the CD74HC238:
HBM: 500V
MM: 200V
CDM: 250V (looks like it was only tested at this level and not higher)
I will forward this post to another team member to help you with the TPS device.
Thanks!
-Karan
Hi Umesh,
I can't find the device datasheet and any Apps engineer in the production line I'm working for; but found the device expert who did answer other customer questions' on e2e before. I've assigned the request to the expert; wish you can get answer after holidays.
Hello Umesh:
Here is the data for TPS65651:
Human Body Model (HBM): 2000V
Charge Device Model (CDM): 500V
Kind Regards,
Liaqat